FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
02-24-2023 06:59 PM
Any ideas why the other languages are not showing up when I add a POU to a PLC Program? I have reinstalled several times, Repaired several times and nothing seems to help. I have also verified that my IndraWorks v14 and v15 Engineering softwares work as they should and show all available languages. The issue is only showing up in CtrlX PLC Engineering. I was thinking maybe a bad install file so I have downloaded the latest files again and still have the issue. Also had an employee install with same files on his computer and he did not have the issue I have. So I am beginning to wonder if it is a .net issue or something local to my computer. Looking for additional ideas outside of what I have tried above.
Solved! Go to Solution.
02-27-2023 08:53 AM
What is the version number of your ctrlX WORKS installation?
02-27-2023 01:10 PM
I have 1.12.7 and 1.12.10 installs and both result in same thing.
04-06-2023 04:22 PM
Hi,
please add the setup log files here. You can find it here : C:\ProgramData\Rexroth\PackageManager\Logs. So zip the folder and add it here.
kind regards
04-06-2023 08:24 PM
Hi,
Issue I believe has been resolved. The computer I was using during that time had a major windows issue and the system actually failed. I have since had my computer replaced. I have installed all the software and had zero issues. Not sure of the specific cause, but I would say it involved something corrupted or missing on my old computer and localized to it.
Thanks