FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-06-2023 11:21 AM
Hello Community,
I'm trying to download CXAC_Base/CXA_CommonTypes/CXA_Utilities/CXA_EthercatMaster libs from CodeSys store, but the download fails with "The download failed". status Any idea from where I can download/install missing libraries?
Solved! Go to Solution.
04-07-2023 08:55 AM
Hello leszekw
This libraries are comming from Rexroth and not from Codesys. So you can't download it at the codesys strore.
This libs are content of the ctrlX PLC engineering installation. If you install ctrlX WORKS with PLC engineering, the libs will be installed automatically.
Regards
Jochen
04-20-2023 11:43 AM
As an addition:
It is at the moment not possible to program a ctrlX CORE with a standard CodeSys installation. You will have to use ctrlX PLC Engineering that is part of ctrlX WORKS.
04-20-2023 11:54 PM
All good now. I moved ctrlX PLC Engineering from V-0116 to V-0112 and project compiles. This would mean that something went wrong during V-0116 installation.