cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

IO Engineering, Can't use Startup Parameters with IndraDrive

IO Engineering, Can't use Startup Parameters with IndraDrive

joeG
Established Member

ctrlXIO 1.14.1

 

I am able to add startup parameters to a ctrlX drive in ctrlX IO. When I try the samething with an IndraDrive I am not able to add any parameters to the startup list.

 

I have attached a picture, when I click OK nothing happens regardless of the name, IDN, bit length and value.

5 REPLIES 5

ChrisLarkin
Established Member

Please follow these steps (see screenshots for reference):

  1. Enable expert settings
  2. Go to Expert Process Data
  3. Select either AT or MDT as required
  4. Select insert
  5. In the pop-up complete information
    1. Name
    2. IDN
    3. Data Type (bit length is auto generated when data type selected)
  6. You must transfer field bus configuration after adding parameters

ChrisLarkin_0-1657104779736.png2022-07-06_11h41_39.png

For Indradrive there is a known bug in the ctrlX IO Engineering that startup parameters cannot be set. I will have to check when it will be fixed.

At the moment you would need to do a workaround by writing it by hand via the ctrlX DRIVE Engineering or writing it via the PLC or data layer while startup.

In the version 1.16 releasing the next days it is possible to add startup parameter by hand. The list will still be empty.

UPDATE: Update: The release 1.16 is now available at the Collaboration Room (PT area)! Please get in contact with your known sales contact person to get access.

joeG
Established Member

@CodeShepherdthanks for the update, that is great news!

 

One of our customers use the IndraDrive and ctrlX Drive with a Beckhoff EtherCAT master. When they are online and add parameters to the startup list it uses the current value, that would be a nice feature to have in the future with the ctrlX.

CodeShepherd
Community Moderator
Community Moderator

Update: The release 1.16 is now available at the Collaboration Room (PT area)! Please get in contact with your known sales contact person to get access.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist