05-20-2021 02:01 PM
I am trying to add the IDE app to my CORE so I can learn Blockly. I have been running versions 21.03.2 and 1.8.3. My CORE was controlling my Cs drive via PLC code for the past week. I have stopped the PLC app. I wanted to try to control the drive with Blockly so I am trying to install "IDE IDE-V-0108.0.arm.app" I downloaded the app on 5/19/2021 from the ctrlX collaboation site. I am in service mode when I try to install the app and I always get a fault that reads "Upload failed! Assertion file missingin app bundle for architecture arm64 One of the provided arguments is invalid"(picture attached). I have the python runtime succesfully installed already. My hardware is R911406308 AB1. Please offer me any suggestions you may have to eliminate this install fault.
Solved! Go to Solution.
05-20-2021 03:25 PM
I would suggest that there was an error while downloading. Did you already try to redownload the file?
Please be aware, that a the moment there are two versions of the IDE App. One .arm.app working for a real ctrlX CORE and another .amd.app for a ctrlX COREvirtual.
I will check the file on the server.
05-20-2021 03:35 PM
I have tried a second download with the same install failure.
I am using the arm version because I have ctrlX CORE hardware.
06-28-2021 09:18 AM
Sorry for the late reply.
Please send me a private message with contact data from your side so we can have a look in a meeting to this topic.
07-02-2021 08:21 AM
Hello RGrieger
There seems to be a problem with the big size of the IDE App. Can you update the Automation Core to version 1.8.2 and try again to install the IDE App.
Regards
Jochen
08-26-2021 04:01 PM
Any news on this or can the topic be closed?
11-25-2021 04:00 PM
Hi Jochen Mueller,
I have the same trouble but with EtherCat App V1.10, it is strange because I was working normally with Virtual CtrlX and CtrlX CORE (not at the same time) but suddenly I cannot work anymore with Virtual CtrlX and EtherCat App V1.10 because this error, I don't know what happen, could you help me?
11-29-2021 07:55 AM
Hello Jacks
I dont think that you have done this at previous versions, because at all versions it wasn't possible to install the Ethercat.app at the virtual control. Currently the Etercat app needs a real hardware.
The requirement is already in the development department, but not priorized yet.
Regards
Jochen