FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-13-2021 12:28 PM - last edited on 10-13-2021 03:44 PM by CodeShepherd
EDIT:
Moved to own topic out of this thread.
Hello ,
finally I got the textual code running but I always get these error while running it. I just took the example from the video description I found on our community and changed the axis an kinematic name in the python code ( see attached screenshot )
Questions:
1. Could you help me to understand while I got the error while running the code ?
2. In the videodescritption the option " Launch python in script engine" is shown to be selected. And if I got it right in the video is selected the engine that was created before using the visual code programmig. Is there a way to start the textual pythion code directly without having to use the visual code before to generate the engine ?
3. Is it possible to start the Textual python code from outside the IDE app ?
4. Is it possible to start the textual python code from the Indralogic PLC App ?? How ??
Many Thanks
Giuseppe
Many Thanks
Solved! Go to Solution.
10-13-2021 04:05 PM - edited 10-19-2021 07:53 AM
B) The error in picture 2021-10-13_12h15_59.png seems to show that someone commanded a stop to the kinematic from outside the script. See error code 0C270309 in the online documentation.