08-20-2020 09:52 AM
A customer has installed ctrlX WORKS inside the Oracle VM VirtualBox 6.1 (Win10). Now we are not able to start the ctrlX CORE virtual. Has anybody experience with that?
Solved! Go to Solution.
08-25-2020 10:06 AM
The custumer itself installed the QEMU (virtualisation software) and manipulated the *.bat file of the virtual control image. I think there is/was a issue with the hardware acceleration settings inside the *.bat file. After that, the custumer was able to start the ctrlX CORE virtual inside a VM with WIN10.
It would be very useful when we provide a solution for this (run ctrlX WORKS/CORE virtual inside a VM). Because a lot of people install software within a VM.
09-01-2020 08:46 AM
Please have a look to the blog "How to set up a ctrlX COREvirtual" for further information or restrictions.
09-01-2020 12:15 PM
It is possible to use the ctrlX virtual inside VirtualBox. But it is very performanceless, because of the missing hardware acceleration.
So if customers don't need performance they can use the virtual control inside VirtualBox.
06-01-2022 09:12 AM
Da steht "solved"!
Wenn ich dem Link folge kann ich keine Lösung entdecken! Oder hab ich da was übersehen?
06-01-2022 09:22 AM
Did you check the notes area at the end of the artikel? There are several hints for different topics.
We added "Windows Hypervisor Platform" as second hardware acceleration method that is supported in many virtualizations.