cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

How to run a ctrlX CORE virtual inside a virtual machine (VM)

How to run a ctrlX CORE virtual inside a virtual machine (VM)

LunatiX
New Contributor

A customer has installed ctrlX WORKS inside the Oracle VM VirtualBox 6.1 (Win10). Now we are not able to start the ctrlX CORE virtual. Has anybody experience with that?

 

5 REPLIES 5

LunatiX
New Contributor

The custumer itself installed the QEMU (virtualisation software) and manipulated the *.bat file of the virtual control image. I think there is/was a issue with the hardware acceleration settings inside the *.bat file. After that, the custumer was able to start the ctrlX CORE virtual inside a VM with WIN10.

It would be very useful when we provide a solution for this (run ctrlX WORKS/CORE virtual inside a VM). Because a lot of people install software within a VM.

CodeShepherd
Community Moderator
Community Moderator

Please have a look to the blog "How to set up a ctrlX COREvirtual" for further information or restrictions.

It is possible to use the ctrlX virtual inside VirtualBox. But it is very performanceless, because of the missing hardware acceleration.

So if customers don't need performance they can use the virtual control inside VirtualBox.

stefanEfg
New Poster

Da steht "solved"! 

Wenn ich dem Link folge kann ich keine Lösung entdecken! Oder hab ich da was übersehen?

Did you check the notes area at the end of the artikel? There are several hints for different topics.

We added "Windows Hypervisor Platform" as second hardware acceleration method that is supported in many virtualizations.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist