How can I run/activate a python script via node-red?
With the description above (YARC) it's possible for me. But I tried it with node-red and our ctrlx-datalayer-request node from node-red-contrib-ctrlx-automation. I try the following:
I did some tests with objects and with string as payload. But I always get the error message:
Any hint's? Thanks.
Additional question...
Do we have to run/activate a python script after every reboot of the control in this way? Or de we provide a mecanism to automaticly run a python script inside the "active solution"? For me it make no sense to program python scripts, which I have to run/activate with another program/interface (REST, node-red, C++, ...).
Solved! Go to Solution.
First you have to choose the payload as "value + type (json)" because you are trying to handle over an complex data type.
Second your payload including the object have to look like this:
var newMsg = {};
newMsg.payload = {};
newMsg.payload.value = {"name":"MyInstance3","language":"python"};
newMsg.payload.type = "object";
return newMsg;
EDIT:
At the moment script instances are not persistent and so get deleted while a reboot. Also there is no automatism to start and run a script. We are already aware of this topic and are working on it.
See also examples in "node-red-contrib-ctrlx-automation". They can be imported in Node-RED directly:
Node-RED import ctrlX AUTOMATION examples
Hi,
you can have the functionality of a persistent python instance by using the init script.
See this post here