Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Error 404 in datalayer when using namespace attribute

Error 404 in datalayer when using namespace attribute

AndyL
Member

Hi,
When using variables with {attribute 'namespace':=''} in the plc the datalayer goes down with error code 404. Is this a known issue or it is not prohibited to do like that?

Kind regards
Anders  

3 REPLIES 3

PedroReboredo
Community Moderator
Community Moderator

Moved to area ctrlX WORKS.

Jochen_Mueller
Community Moderator
Community Moderator

I have tried it with the version 01V06 (RM20.11).

If I use the namespace attribute my variables doesn't appear in the datalayer. So it seems we have a problem. I forward this issue to the development department...

Funktionality with RM21.11 (V1.12)

  • Add "Symbol-Configuration" to application
  • use {attribute 'symbol' := 'readwrite'}
  • use {attribute 'namespace' := 'Application.xyz'}

the first part of the namespace string must be the name of the Application (here Application :-))

The following parts defines the namespace with which the GVL appears at the datalayer. The basic path (plc/app/"Application-Name"/sym/) is always fix. Means you can only influence the path after the basic path.

Jochen_Mueller_0-1647596846161.png

 

Jochen_Mueller_1-1647596866416.png

Regards

Jochen

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist