FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
12-16-2020 04:59 PM
Hi,
When using variables with {attribute 'namespace':=''} in the plc the datalayer goes down with error code 404. Is this a known issue or it is not prohibited to do like that?
Kind regards
Anders
Solved! Go to Solution.
12-18-2020 11:18 AM
Moved to area ctrlX WORKS.
01-19-2021 08:24 AM
I have tried it with the version 01V06 (RM20.11).
If I use the namespace attribute my variables doesn't appear in the datalayer. So it seems we have a problem. I forward this issue to the development department...
03-18-2022 10:50 AM
Funktionality with RM21.11 (V1.12)
the first part of the namespace string must be the name of the Application (here Application :-))
The following parts defines the namespace with which the GVL appears at the datalayer. The basic path (plc/app/"Application-Name"/sym/) is always fix. Means you can only influence the path after the basic path.
Regards
Jochen