FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
08-08-2024 01:05 PM
Hello everyone!
I am in a Delta robot project, and I have an issue. In IDE, when I want to run any program (doesn´t matters if it includes motion or not), I send me this:
When I check the logbook, I find the following image:
These are the app I´m using:
I can move with comissioning option the full kinematic, but not through the IDE.
Do enybody knows what could be happening here?
Best regards.
08-08-2024 03:00 PM
May be this is a problem with the versions you use. System seems to be 2.4 and IDE 1.20
08-08-2024 03:45 PM
Hi, how are you?
It seems to be the lastest version for my country...
08-08-2024 05:13 PM
Hi @ElCazita ,
Please use the latest version of the IDE app with the v2 system apps. I'm fairly certain this is a version incompatability as stated by @Michael_A. I'm sorry it does not seem to be available in your country collaboration rooms. Do you have an early access account?
Also, how are you trying to execute the script? If you are not attaching to a script interpreter instance, similar problems could occur.
08-09-2024 10:54 AM
It should be a Problem with the versions you are using. v1.20.58 is only compatible with other apps of version 1.20.
09-02-2024 02:08 PM - edited 09-02-2024 02:09 PM
As an information, version 2.6 of cttrlX AUTOMATION IDE App is available now for download. Please repeat your test with this version an tell us if it now working.