Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

10-day "Temporary usage rights" with RM21.11

10-day "Temporary usage rights" with RM21.11

bschmidt
New Contributor

Hello,

Before applying my purchased licenses to my ctrlX CORE I wanted to see what is possible if the 10-day temporary usage rights is switched on. This allowed me to use Motion, IDE, Node Red without licence. But PLC and EtherCAT still showed the "not licensed" message, so I could not do anything with these critical apps. Is this a bug, or is it really the case that there will not be a trial period for those apps?

Best regards,

Brian

7 REPLIES 7

PedroReboredo
Community Moderator
Community Moderator

Hi Brian,

are you talking about the Trial License you activated in the Licensing Center?

Please send some screenshots / more information. 

Cheers, Pedro

Hi Pedro,

I'm sorry for the confusion, I meant to say "10 day" not "10 hour". I will edit the original message after this reply. This is activated in the licensing area of the ctrlX CORE. Please see screenshots below.

Best regards,

Brian

bschmidt_0-1640272325012.png

bschmidt_1-1640272387670.png

bschmidt_2-1640272435105.png

bschmidt_3-1640272472298.png

bschmidt_4-1640272522488.png

 

After following path above, Motion is working (for example), but PLC and EtherCAT are still blocked:

bschmidt_5-1640272592371.png

bschmidt_6-1640272622788.png

 

 

 

 

 

 

 

 

Hi Brian,

thanks for the additional information, now I understood.

The temporary usage rights are kind of an emergency mode, and can only be activated once. This should also include licenses for the ctrlX EtherCAT Master and PLC App. I've opened a ticket to solve that. Sorry for the inconvenience.

But, have a close look under the christmas tree... 🙂 You should really use the Trial License for your use case which you already have within the Licensing Center, and can assign to your device (map entitlement). I double-checked that, both PLC and EtherCAT Master app licenses are included.

Hope I could help, if not give me a sign.

Regards,
Pedro

Hi Pedro,

Thank you, I will check into the trial license in the Licensing Center. Good to know PLC and EtherCAT Master will be added to temporary usage. I think this feature will be used quite frequently until more people get familiar with the Licesning Center.

Best regards,

Brian

hi pedroReboredo

I have another problem about the 10-day "tempprary usage rights".I have a new ctrlx core and purchased licenses .

first,I applying apart of licenses and it's ok.

secondy,I enable the 10-day "tempprary usage rights"

third,I appying all of license,then,an error is occur,following screenshot is error message:

LZT_0-1651025862865.png

then refresh web ,web display the following message:

LZT_1-1651026059293.png

meanwhile, three more license in license file:

LZT_3-1651026473288.png

then,reload system is necessary and cann't applying all of licenses again(because the same error will be occur)

now,can i applying  all of licenses again until may 3.022 only(temporary usage rights end date)?Is there any other solutions?

thanks for your support.

CodeShepherd
Community Moderator
Community Moderator

@LZT I will get in contact with you directly and we will investigate this.

Please don't mix up the two different possibilities of getting temporary licenses:

  1. Temporary usage rights can be activated once each hardware e.g. for exchange purposes. The time will start in the moment you click the button in the ctrlX CORE:
    activate temporary usage rightsactivate temporary usage rights

  2. Trial licenses can be found via the licensing center and can be used several times. Like on your screenshot. Their time is running from the moment on you download the license from the portal:

    LZT_3-1651026473288.png

thanks for your answer.

enable the temporary usage rigths was a unexpected operation,it won't happan again!

it has been sloved temprorarily,

thanks for your support again

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist