FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
01-10-2024 04:24 PM - edited 01-10-2024 04:26 PM
Hello,
After installing the correct SAFEX-C1x device description file for the running firmware\FPGA we still had the 0x001E: Invalid Input Configuration. What we found was the elements for the FSoE Master Connections did not get installed:
After several attempts of uninstalling - reinstalling we exported the missing elements from another PC and installed them manually, this process worked:
Here is some additional information about the PC and I/O Engineering:
Solved! Go to Solution.
01-14-2024 07:19 PM - edited 01-14-2024 07:21 PM
Hello,
you have both files on your PC. It's important, as I know.
You have to install just the first file "BoschRexroth_ctrlX_SAFETY_SAFEX_C12_C15_ECAT.xml" !!!
but also need the second file to be on your PC (BoschRexroth_ctrlX_SAFETY_SAFEX_C12_C15_ModulesECAT.xml)
Regards,
Stefan
01-16-2024 03:08 PM
Hello stefanAT_ctrlX,
Thank you for the information. Both files were in the same folder. We also tried installing the BoschRexroth_ctrlX_SAFETY_SAFEX_C12_C15_ModulesECAT.xml manually.
Are the FSoE Master connections installed from the BoschRexroth_ctrlX_SAFETY_SAFEX_C12_C15_ModulesECAT.xml or BoschRexroth_ctrlX_SAFETY_SAFEX_C12_C15_ECAT.xml file?
Are the FSoE Master and FSoE Slave connections installed from different XML files or are the FSoE Master and Slave connections installed from the same XML file? The FSoE Slave connections did get installed, just the FSoE Master connections were not installed.
Is there an overview of which elements are installed with each XML file?
01-18-2024 03:38 AM - edited 01-18-2024 03:40 AM
Hello@ctrlXProgrammatore ,
Let us know whether this helped or not.
Best regards
Your ctrlX SAFETY team
01-18-2024 02:15 PM
Hello @AllAutomation,
Thank you for the information. With these details and some additional testing, I have a better idea of the "0x001E: Invalid Input Configuration" error we saw.
I did want to let others know about the missing installed FSoE Master Connections but based on your explanation it was probably not related to the "0x001E: Invalid Input Configuration" error we had.
What would be the issue or when would this become an issue if the three FSoE Master Connections shown above are not installed?
08-23-2024 02:43 PM
Hello,
your description saved my day 🙂
After many hours of struggling and searching through How-to and documentation I realized why I got "0x001E: Invalid Input Configuration".
I assume it would be useful to add it to any how-to where drives (and other slaves) are configured because it´s very helpful information which you cannot easily find anywhere.
Thx