FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
10-22-2024 02:15 AM
On a machine with 8 safeX C.15 talking over SMMC, occasionally one of them will get an F3232 fault. Nothing stands out on the 24V wiring side. The same 24V power supply is used for two safeX C.15. If the issue was the power supply, I'd expect both safeX to get the fault. On an identical machine I replaced the safeX and the issue never came back. This machine got the fault on a different portion of the system, so no common factor there. Are there any troubleshooting steps I should try besides replacing the device? Device firmware is 1.0.1.47. Safety Engineering version is 1.8.3.
a month ago
Please can you post the following information:
Thank you!
PS: check your used ctrlX SAFETY Engineering Version and correct it in your post above - the last digitbundle is missed (1.8.3.?)
3 weeks ago
Hi there,
I was given the information above from a customer that was on site. They're replaced the unit and set aside the one that was generating the fault. If I can get the requested info, I'll pass it on.