FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
05-30-2022 05:11 AM - last edited on 05-30-2022 08:55 AM by HmiGuide
I try use CtrlX CORE virtual to run Modbus TCP server with IL_ModbusTCPServer, it work normal in beginning.
But the Plc task will jump watchdog exception after it worked for some time(random).
I already set the cycle time to 20ms and set sensitivity to 5 but it still happening.
I check the process time by IL_HighResTimeDiff, looks like the maximum time will get bigger and bigger after for a long time.
Is this normal because I running in the virtual CtrlX CORE?
Solved! Go to Solution.
05-31-2022 08:39 AM
The ctrlX core virtual is not a real time operating system, you should run it without watchdog.
05-31-2022 09:05 AM
Ok, understood.
Thank you for the help!