Hello,
On the ctrlX Core, within the PLC app, we can use PID function blocks or other functions that are available for XM and CML plc's?
Are these functions available?
Solved! Go to Solution.
Hello Vlad
the control FBs are available
### Update 19.07.2022 ###
with the version 1.14 you see the library only if you activate the option "Display advanced library". With version 1.16 the activation of this option is not necessary anymore.
The way via "Advanced" button on the left botton side of the dialog is not recommended, because the libs are not add as placeholder, which cause problems if you up-/downgrade the project version.
Regards
Jochen
Thank you for informations.