cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

ctrlX PLC - PID functions

ctrlX PLC - PID functions

vlad
Established Member

Hello,

On the ctrlX Core, within the PLC app, we can use PID function blocks or other functions that are available for XM and CML plc's?

Are these functions available?

2 REPLIES 2

Jochen_Mueller
Community Moderator
Community Moderator

Hello Vlad

the control FBs are available

Jochen_Mueller_1-1658156882724.png

 

### Update 19.07.2022 ###

with the version 1.14 you see the library only if you activate the option "Display advanced library". With version 1.16 the activation of this option is not necessary anymore.

Jochen_Mueller_1-1658210177332.png

The way via "Advanced" button on the left botton side of the dialog is not recommended, because the libs are not add as placeholder, which cause problems if you up-/downgrade the project version.

 

Regards

Jochen

 

vlad
Established Member

Thank you for informations.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist