FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-20-2023 06:59 AM
Hi , i would like to implement the function "SysGetTimeUs", why is it showing error stating that it is not defined? It is acting fine in my indraworks, but not ctrlX plc. could it be that i have to sign the cert? if yes, then where can i configure ?
P/S: this error pops up when i try to import the project file from Indraworks.
Solved! Go to Solution.
02-20-2023 08:29 AM - edited 02-20-2023 08:30 AM
Just tested it on my side and it is working. Could you try to generate code and see if error will be gone?
02-20-2023 08:35 AM
02-20-2023 09:03 AM
could you send me your project archive or at least an export of the part the code is part of as a private message, so I can have a look to it? And please also tell us the version of ctrlX WORKS you are using. I tested it in 1.18.0
04-24-2023 10:37 AM
Is this still an issue or can this topic be closed?
05-02-2023 02:21 AM
Hello, Yes you may close this topic. Thank you.
05-02-2023 08:11 AM
Could you share with the community how you solved it?
05-02-2023 09:12 AM
Managed to get it solved by clicking the "Add Library" tab under Library Manager , go to "advanced" and search for the the feature that you wish to import into the library.