Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Using function from the library (restricted by signed cert?)

Using function from the library (restricted by signed cert?)

Mr_Wonder_Why
Established Member

Hi , i would like to implement the function "SysGetTimeUs", why is it showing error stating that it is not defined? It is acting fine in my indraworks, but not ctrlX plc. could it be that i have to sign the cert? if yes, then where can i configure ?

 

P/S: this error pops up when i try to import the project file from Indraworks. 

7 REPLIES 7

CodeShepherd
Community Moderator
Community Moderator

Just tested it on my side and it is working. Could you try to generate code and see if error will be gone?

ctrlX PLC Engineering SysTimeGetUsctrlX PLC Engineering SysTimeGetUs

Hi i am still getting the same error here.

could you send me your project archive or at least an export of the part the code is part of as a private message, so I can have a look to it? And please also tell us the version of ctrlX WORKS you are using. I tested it in 1.18.0

Is this still an issue or can this topic be closed?

Hello, Yes you may close this topic. Thank you.

Could you share with the community how you solved it?

Mr_Wonder_Why
Established Member

Managed to get it solved by clicking the "Add Library" tab under Library Manager , go to "advanced" and search for the the feature that you wish to import into the library.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist