The Address is Already Used

The Address is Already Used

EngJay
Long-established Member

 

I was using the PLC Datalayer_Realtime feature 'Select realtime data' -> 'selectively from the core' to add status words and dc bus control word for multiple drives. 

As you can see in the screen shot below, I get the errors ctrlX_DRIVE_XMD_SoE_1_2_FSoE_7: The address %IW224 is already used and ctrlX_DRIVE_XMD_SoE_1_2_FSoE_7: The address %IW226 is already used.

There seems to be a bug where the address locations are not properly auto-assigned and for some reason at this point it reuses the address location of ctrlX_DRIVE_XMD_SoE_2_2_FSoE_6.

I'm using PLC Engineering version 2.4 and attached the version info for reference.

EngJay_0-1705448003062.png

 

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

Sorry for the late reply.

Did you try a clean all of the project to get rid of any artifacts?

We are currently reworking the address ordering mechanism because of problems with special third party modules. And as I could not reproduce the problem, could you do a test with version 2.06 coming up end or March and see if it working there?

EngJay
Long-established Member

If memory serves, I did try to clean all, but I will review to be sure.  For now, of course, I was able to manually assign an open address.  I will look to test again with 2.06 in March and update the post.  Thanks.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist