01-17-2024 12:36 AM
I was using the PLC Datalayer_Realtime feature 'Select realtime data' -> 'selectively from the core' to add status words and dc bus control word for multiple drives.
As you can see in the screen shot below, I get the errors ctrlX_DRIVE_XMD_SoE_1_2_FSoE_7: The address %IW224 is already used and ctrlX_DRIVE_XMD_SoE_1_2_FSoE_7: The address %IW226 is already used.
There seems to be a bug where the address locations are not properly auto-assigned and for some reason at this point it reuses the address location of ctrlX_DRIVE_XMD_SoE_2_2_FSoE_6.
I'm using PLC Engineering version 2.4 and attached the version info for reference.
Solved! Go to Solution.
02-01-2024 02:04 PM
Sorry for the late reply.
Did you try a clean all of the project to get rid of any artifacts?
We are currently reworking the address ordering mechanism because of problems with special third party modules. And as I could not reproduce the problem, could you do a test with version 2.06 coming up end or March and see if it working there?
02-01-2024 04:53 PM
If memory serves, I did try to clean all, but I will review to be sure. For now, of course, I was able to manually assign an open address. I will look to test again with 2.06 in March and update the post. Thanks.