01-26-2024 12:06 PM - edited 01-29-2024 10:03 AM
Hi
Version: 2.04
I'm having trouble assigning a task to a specific core, had no problem in v1.x. The error occurs when there are several PLCs in the project. An error occurs when trying to download. Converted project from 1.20.
Same error if i try with "core 2". If i use "Fixed pinned" it works, but the application running on Core2.
Reproduce the error with new project
I manage to get the same problem with new project. using 1 physical CtrlX X3.
Is this a CoDeSys thing?
It seems to work better if CtrlXs in the project has real connection to its CtrlX. Then download works with coreassignment.
But if i have 2 physical CtrlX and I disconnect the network cable from one, I get the same error when I try to download to the other.
What is happening?? Is this a known problem?
Solved! Go to Solution.
02-21-2024 09:00 AM
Hi,
this sounds strange. We'll check this issue.
kind regards
03-22-2024 03:17 PM
Any news here? Is this still an issue?