cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Problem trying to connect to the PLC

Problem trying to connect to the PLC

Fred74
Established Member

Hello,

I am working with CtlrxWorks 1.6.0

When I open Indralogic from the webInterface I got this screen

Fred74_0-1610989043157.png

The only way I have is to press the right button.

After pressing it I got the following screen : no possible to go online with the PLC see the follonwing screen

Fred74_1-1610989177258.png

 

Fred74_2-1610989189851.png

 

How can I get rid of that?

I tried to cancel the right field but nothing is working.

I tried also to stop the virtual control 

and also tried to reboot the PC 

No way.

 

Thank you very much for your support.

 

Frédéric

1 REPLY 1

FooFighter
Long-established Member

Hello Frédéric,

in Version WRK-V-0106 there exists a bug opening a synchronized project from the control in the webbrowser opend via the IpV6.

A workaround is to start the browser with the IpV4 address.

The second problem is that the PLC Address of the control is not set correctly. Try to enter the IpV4 address into the field below the control in the communication settings page (double click on the controller in PLC Engineering).

The third problem can be solved by activating encrypted communication for the control. (Should be activated by default).

Refer to Encrypting Communication, Changing Security Settings 

Regards, Oliver

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist