FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
08-08-2024 08:29 AM
Hi,
I get the following error when i'm trying to connect to the core. The designer does go online after pressing ok.
Making an online change does work but saving and/or archiving the project doesn't work.
It seems to be stuck at the following auxiliary file.
This issue is only happening when i'm on the same network as the core. If i disconnect from the network and try to save/archive there is no issue. could it be that the core is corrupt. or that the bootproject on the core is corrupt?
Solved! Go to Solution.
08-20-2024 01:12 PM
Because of the error message concerning the IP address, we checked the communication settings.
We discovered an explenation mark with the message like the example below:
After applying the IP address of the control was applied to the date on the control and the problem was solved.