cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

PLC project save error

PLC project save error

DdG
Established Member

Hi,

I get the following error when i'm trying to connect to the core. The designer does go online after pressing ok.DdG_0-1723098164036.png

Making an online change does work but saving and/or archiving the project doesn't work. DdG_1-1723098164037.png

It seems to be stuck at the following auxiliary file.

DdG_2-1723098164037.png

 

This issue is only happening when i'm on the same network as the core. If i disconnect from the network and try to save/archive there is no issue. could it be that the core is corrupt. or that the bootproject on the core is corrupt?

1 REPLY 1

Mike_T
Member

Because of the error message concerning the IP address, we checked the communication settings.

We discovered an explenation mark with the message like the example below:

Mike_T_1-1724152341838.png

 

After applying the IP address of the control was applied to the date on the control and the problem was solved.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist