PLC not starting on power up

PLC not starting on power up

aFouraker
Occasional Contributor

Hello, when starting the core the PLC application does not start. I have to manually start the application and then it runs. Is there a setting to make it run on startup? 

4 REPLIES 4

Sgilk
Frequent Contributor

Hi Alex @aFouraker ,

You'll want to make sure the application is set as a boot application in the controller. In PLC engineering, you can select "Create boot application" while online with the controller and it should do the trick. 

Sgilk_1-1708113416824.png

If you have a different project and want to overwrite the boot application, you can go online and select the "Update boot application" checkbox.

Sgilk_0-1708113358139.png

Hello, We have switched off on the same issue, it is the boot application, any other reason this could occur?

Could a missing node in the datalayer cause this?

Mike_T
Member

Hello,


My customer has the same problem.

Mike_T_0-1710243962219.png

 

Is there a known solution?

 

Regards, Mike

Hey Mike,

I had to do a clean install of the OS (from SD card) then load the PLC program from a download and not a restore and it worked 

Hope this helps

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist