Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Modbus IL_ModBusTCPClient connection problem

Modbus IL_ModBusTCPClient connection problem

Chirag03
Established Member

Hello ,

I am using ctrlx PLC 1.20.4 and works 1.20.2  . I  try to connect modbus communication via IL_ModbusTCPClient function block . In which  Enable is true but InOperation is not true. I am not able to communicate with specify address but, i can ping this address via command prompt. Previously it was working fine but, now it is not showing InOperation true . Please see  attached picture for your reference  and give me solution. 

 

 

2 REPLIES 2

HmiGuide
Community Moderator
Community Moderator

When you can't connect you should check the following:

  • Is the Modbus server running
  • Is the ip and port correct
  • are there any firewall settings (or e.g. VPN connections), which blocks the connection

You said it was working. What did you change since it is not working anymore?

JordiLaboria
Established Member

Good morning

See if these manuals on Modbus communication between XM and ctrlX Core is helpful.

We have even used this to pass states from the IOs in Ethercat to the XM

Best Regards

 

Jordi Laboria

E-Mail: jordi.laboria@boschrexroth.es

https://www.youtube.com/channel/UCzE-ieCIkyMsuvyE0UDji9g

DCET/SLF4-ES

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist