cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Missing plug-in 4.0.0.0 error opening ctrlX PLC Engineering 1.12.0

Missing plug-in 4.0.0.0 error opening ctrlX PLC Engineering 1.12.0

bschmidt
New Contributor

Hello,

Since updating to ctrlx WORKS 1.12 I am always getting the error below when I open PLC Engineering. If I click 'No" to the message I can make a new project, but then I get an error message when I complile (see below).

I have tried multiple times uninstalling and reinstalling ctrlX WORKS but always run into the same issue.  If I install ctrlX WORKS 1.12 on a Win10 virtual machine, I do not get this error.  So I guess there is a unique problem on my Win10 host operating system. But if I reinstall ctrlX WORKS 1.10 on my host operating system, that one is still working fine. 

bschmidt_0-1638892297722.png

bschmidt_1-1638892405495.png

Best regards,

Brian

6 REPLIES 6

Jochen_Mueller
Community Moderator
Community Moderator

Hello Brian

it is a known problem with Bosch PC after the automatic Update of an Outlook Addin. 

Workaround:

Copy the attached file (PW: Bosch) SQLite.Interop.dll to the folder <Installationpath>\Studio\Common and start repair-Installation

Regards

Jochen

Hello Jochen,

That fixed it - thank you!

Best regards,

Brian

Hi Jochen,

I've recieve the error message below, which looks similar/the same as the other message in the original post.
However I've tried your solution with the dll and repair-installtion but I still recieve the error.
I'm running 1.10.6 on Windows 10 host machine.

ChrisLarkin_1-1639048702709.png

 

 

Hello Chris

Does this message occur suddenly at a working version?

Or does it appear with a new installation of ctrlX WORKS? At a new installation please make a repair of this.

Regards

Jochen

Hi Jochen,

It is a new install.
I had 1.12.0 installed to check for some updates, however I then back-dated the version to 1.10.6 to continue some work started in that version.

I have copied the dll to the correct location and performed a repair on the current install, but I still recieve the error message.

Hi ChrisLarkin,

it is solved with version 1.12.2 you can get it in the collaboration room.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist