FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
05-09-2023 10:59 AM
Hello,
There is a way to use the Torque Control, programming with AxisInterface and the Motion app.
Is it possible to change the operation mode manually on the Drive to select torque control and do the rest of the programming with AxisInterface?
If I add the power control in the Datalayer of the PLC, AxisInterface does not work and I cannot force the operation mode.
Thanks in Advance.
Solved! Go to Solution.
06-15-2023 07:14 AM
Hello,
until now it is not possible to use torque mode with axisinterface beacuse there are no commands for torque implemented in the motion.
The only way to use torque in the drive would be to handle the drive as an io and control it completely from plc side.
06-15-2023 10:20 AM
Hello Michael_A,
Thank you for your resply.
Is there a plan to implement it in the future?
06-16-2023 06:29 AM
Hello David
The realization of the torque mode within the motion app (and the additional PLC support PLCopenFB, MotionInterface) is planned for the RM 24.07. If this feature really come will be decided beginn of 2024.
Regards
Jochen
03-29-2024 02:47 PM
Hello @Jochen_Mueller ,
Is torque mode still on the roadmap for RM24.07 in the Motion app?
a week ago
Yes, it is still planned for ctrlX MOTION 3.2 coming up end of July 2024.