09-22-2020 07:16 AM
Hello
I am getting Error "SAM - 090F2001 - DL_SUBMODULE_FAILURE" While Grouping Axis
Could not find Description of the error
Please suggest
Thanks and Regards
Samkarshan V
Solved! Go to Solution.
09-22-2020 08:16 AM
This is a general error that means that the object you like to command is not ready to do so.
Please beware that axis have to be enabled (AF/AH) before they can be added to a kinematic.
How do you send the command? Via the WebInterface?
09-23-2020 12:55 PM - edited 09-23-2020 12:56 PM
I have added 2 indraCs drive to ctrlX core and 1ctrlX slave.in total 4 axes
This problem occurs only when ctrlX slave drive is added to kinematic and when grouped.
drives are grouped after power on only
Yes i command from web interface
09-23-2020 07:40 PM - edited 10-02-2020 01:00 PM
Please contact a kolleague of the sales technical support (STS) directly for forther investigation.
10-02-2020 12:57 PM
In the ctrlX MOTION version 1.0.4 it is not possible to group an robot when an axis is matched to the meaning "MAIN_AXIS_A", "MAIN_AXIS_B" or "MAIN_AXIS_C".
If you need have auxiliary axis please use the meaning "FREE_AXIS_x".