Motion Interface 2.6 -> FixedStop

Motion Interface 2.6 -> FixedStop

nishimura
Established Member

Hi!

I am trying to command an axis within a PLC app. The idea is to use a Fixed Stop command.

But whenever i use the command, the axis gets an error : 0C560100. 

nishimura_0-1722945322182.png

Any idea of what i might be doing wrong?

3 REPLIES 3

Michael_A
New Contributor

Hello, did you mapp the parameter S-0-0080 and S-0-0084  in the cyclic data of the drive and are they mapped in the axisprofile?
The command has to be buffered.

nishimura
Established Member

Both parameters are mapped. I also now included the torque operation mode on the drive side (after reading the documentation this seems necessary). I tried buffered commands with no sucess.  

Can you check parameter S-0-0124 standstill window of your drive. If i command the fixed stop with a velocity value below this parameter i get an error too. But if i command with a value above the standstill window it works.
If this is not the cause, then please send me the configuration data, the IO-project, the plc project and the logfile.

regards Michael

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist