09-05-2024 02:17 PM
Hi,
Are there any limitations in number of commands buffered in one contour?
and second question:
In case, when we will have "big" buffer of commands, can we start the contour and add new command at the same time, during realizing contour ? something like fifo?
or we have to load complete contour before we will start movement, as it is described in this thread?
09-05-2024 02:38 PM
Please have a look to the topic "limit of commandos used for a contour".
The motion command buffer is always first in, first out and commands can be added while kinematic is already moving at least since version 2.6 of the ctrlX AUTOMATION - Motion app. I will change the explanation in the thread mentioned by you.
09-05-2024 03:03 PM
Thank you for answer.
It will be helpfull if you will give us similar list of commands in correct order, as it is in this thread
09-09-2024 08:55 AM
It is quite the same order. Please have a look to post "ML_KinPolyTransP and ST_CONTINUOUS_SLOPE".
10-22-2024 02:36 AM
Hello,
I used 3000 moves documented in the following post.