FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
06-05-2024 02:02 AM - last edited a week ago by MichaelB
Hi CodeSheperd,
Is there a limit to the number of commands used in a contour? I need to issue over 2000 moves from a custom points table...
Solved! Go to Solution.
06-05-2024 07:26 AM - edited 06-05-2024 07:29 AM
Moved to own topic from "ML_KinPolyTransP and ST_CONTINUOUS_SLOPE".
Which version are you using? In general the available memory is the limit but from version 2.6 there is a setting "motion/kin/<name of kinematik>/cfg/prep-limits/max-cmds-in-buffer" capable of limiting, preventing the system from crashing when out of memory. But 2000 commands are no problem at all.
06-05-2024 07:31 AM
I am using 2.6. I will try to adjust this value and see what happens.