06-24-2022 02:56 AM
Hello,
Our test CtrlX Core is running with PLC Basic license which only allow single task at time.
Now we use the motion interface template, and it created a motion task with TASK_EXTERNAL_EVENT_07 to run the AxisInterface.
My question is:
1. Is this task similar to the motion kernel which in the MLC before?
2. So if this is the task similar to the motion kernel, it means I should use the license with upper then the PLC Stantard?
Or I can run this motion interface in single task project? how to modify the task?
Thank you
Solved! Go to Solution.
06-24-2022 10:01 AM - edited 06-24-2022 10:05 AM
You can use the motion interface with PLC standard and one task also. Simply drag the second program call to the first task and delete the second task.
06-27-2022 08:20 AM
Got it, thank you for your reply.