cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Is single task can run motion interface?

Is single task can run motion interface?

WenKuei
Established Member

Hello,

Our test CtrlX Core is running with PLC Basic license which only allow single task at time.

Now we use the motion interface template, and it created a motion task with TASK_EXTERNAL_EVENT_07 to run the AxisInterface.

My question is:

1. Is this task similar to the motion kernel which in the MLC before?

2. So if this is the task similar to the motion kernel, it means I should use the license with upper then the PLC Stantard?

    Or I can run this motion interface in single task project? how to modify the task? 

 

Thank you

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

You can use the motion interface with PLC standard and one task also. Simply drag the second program call to the first task and delete the second task.

PLC Engineering MotionInterface templatePLC Engineering MotionInterface template

Got it, thank you for your reply.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist