cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

How to achieve Kinematics fast stop?

How to achieve Kinematics fast stop?

KangZhihao
Established Member

I use kinematics move command to achieve position control. I can see there is a ML_KinAbort command to stop the movement. But in ML_KinAbort, there is no deceleration that can be set, so kinematics stops by the last position command deceleration. 

KangZhihao_1-1667877551181.png

In some situation, I want to stop the kinematics in faster deceleration, not by the last position command deceleration setting. I can see the ML_AxsAbort provides the deceleration setting, so in single axis motion control, it can be stopped in fast deceleration. When I use ML_AxsAbort in kinematics, it will cause the error because the axis is in kinematics group state. I don't want to cause this kind of erro in motion control.

KangZhihao_0-1667877504306.png

So how can I achieve the fast stop with deceleration setting in kinematics?

3 REPLIES 3

Michael_A
Long-established Member

As i know this function will come with Release 1.18 -> ML_KinAbort2 (FUN)

So, the abort2 is not released yet? I don't see it in the PLC library or C++ SDK motion command interface.  How long do I need to wait untill the release.

The release of version 1.18 is planned end of this month (november).

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist