FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-15-2024 12:40 PM
The actual topylogy is following:
i can automatically scan these I/Os in I/O Enigeering(Correct sequence)
In WebIU . I saw the topylogy is following:(Correct sequence)
But the topylogy is following inPLC Enigeering
Compared I/O enigeering with PLC enigeering:
Could i do some actions and get correct topylogy in PLC enigeering?
04-15-2024 01:08 PM
Hallo,
Everything is sorted by alphabet in the PLC.
Regards
04-15-2024 01:08 PM - edited 04-15-2024 01:12 PM
There are two possible views in the ctrlX PLC Engineering and it is depending which one is active on your side. In "DataLayer view" it is sorted alpha numeric and in "I/O view" like in the ctrlX IO Engineering.
ctrlX PLC Engineering switch real time data to IO view
ctrlX PLC Engineering switch real time data to Data Layer view
See also thread "Import I/O Modular Device Profile".