FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
04-24-2023 03:18 PM
Hello ,
Will the Ctrlx provided with a CAN-Module in the future ?
Best regards ,
Mesut
Solved! Go to Solution.
04-25-2023 07:29 AM
Hello Mesut,
there are currenty no plannig for an CAN Interface for ctrlX I/O.
What kind of application needs this functionality?
Best regards,
Thomas
06-19-2023 04:31 PM
I know this is a rather old thread.
We have customers who would need a CAN module (CANOpen, J1939, among other commonly used mobile frameworks) to test their valves using hardware that would typically be used to run their valves. These valve drivers most commonly use CAN for communication with the ERC.
I would be nice to have a single package that allows us to fill these needs, there are other solutions of course. It is always better to have a single I/O setup.
06-29-2023 02:38 PM
Hello Thomas ,
Its for a mobile crane that works with Elion rexroth inverter , as i have only CAN Interface on the Elion inverter i must use CAN on CtrlX , other option is to use a CAN to Profinet Converter , but the customer don't like to work with converters ..
08-04-2023 05:34 PM
We build sawmill equipment, we use Sure Grip Controls for operator controls, and like JoshS said we use hyd valve drivers that communicate vs J1939.
See attached example of a joystick that we use on our machines, this joystick has 21 buttons and X-Y axis proportional control. Using CANbus we need only 5 wires for this joystick, instead of 21 digital inputs, and 2 analog inputs when hardwired back to the PLC.
It would be nice to have a single PLC instead of an additional CAN to Ethernet Bridgeway.
10-27-2023 09:48 AM
Hello ,
i see that there is a RS-485 module for the CtrlX Core , but i think this is not for CAN ? .
Best Regards,
Mesut
10-27-2023 03:21 PM
Hello,
I had a lot of success with this adapter. I read then decoded the CAN data over serial in Node-RED. I will link a post on the subject when it is published.
This adapter is also supported at the device driver level, but requires a lot more software overhead and is probably not feasible for most customers at this point.
10-27-2023 03:28 PM
Hi ,
Thanks for sharing your solution , but i prefer the CAN direct on the CtrlX , usb is not so robust connection .
10-30-2023 08:52 AM
Like mentioned above there are no plans for a CAN IO on ctrlX CORE.