cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Add IO-link device to Rexroth S20 module

Add IO-link device to Rexroth S20 module

OpconUser
Member

 

Hello. I have Rexroth S20 IO-link module and I would like to add an actuator to it.

I have IODD xml description file from actuator's manufacturer. Unfortunately I couldn't find any button to add a slot or something like this. Could somebody help with this topic?

OpconUser_0-1668591078144.png

4 REPLIES 4

Sozu
Community Moderator
Community Moderator

Hello,
Currently we do not support IODD files for our S20 IO-Link module.

Regards

Thank you for the answer!

How can we communicate in this case? Is there any possibility?

cc2go
Occasional Contributor

Process data communication is possible without the IODD.
The porcess data mapping, where your data are, you can mostly find in the docu of the IO-Link devices.

Depending on the EtherCAT IO-Link Master, it's possible with the manufacture tools to set parameters in the IO-Link devices.

cc2go
Occasional Contributor

With ctrlX Works v1.18 we provide with the CXA_S20 library a function block to configure the ports of the S20-IOL-8 module with the S20-EC-BK

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist