FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
11-16-2022 10:35 AM
Hello. I have Rexroth S20 IO-link module and I would like to add an actuator to it.
I have IODD xml description file from actuator's manufacturer. Unfortunately I couldn't find any button to add a slot or something like this. Could somebody help with this topic?
Solved! Go to Solution.
11-16-2022 12:00 PM
Hello,
Currently we do not support IODD files for our S20 IO-Link module.
Regards
11-21-2022 11:50 AM
Thank you for the answer!
How can we communicate in this case? Is there any possibility?
11-25-2022 11:26 PM
Process data communication is possible without the IODD.
The porcess data mapping, where your data are, you can mostly find in the docu of the IO-Link devices.
Depending on the EtherCAT IO-Link Master, it's possible with the manufacture tools to set parameters in the IO-Link devices.
12-19-2022 01:42 PM
With ctrlX Works v1.18 we provide with the CXA_S20 library a function block to configure the ports of the S20-IOL-8 module with the S20-EC-BK