cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Static IP Address WebPanel WR21

maurusbien
Established Member

Static IP Address WebPanel WR21

Hello,
Unfortunately I am not able to assign a static IP address to my WebPanel WR21. After I assigned a static IP address to the device via the settings, it seems to be overwritten again. After saving and opening the IP settings for e.g. ETH1 again everything is empty. Also a connection to my ctrlX CORE, which is in the same network via the Chromium web browser of the WR21 is not possible. A ping from my computer to the WR21 is also not possible. How can I assign a static IP address to an WR21 WebPanel?

Tags (3)
3 REPLIES 3
Open
New Contributor

Re: Static IP Address WebPanel WR21

Hello maurusbien,

Try assigning ETH1 and connect your cable to ETH2 in WR21.

 

alink
Long-established Member

Re: Static IP Address WebPanel WR21

Hello maurusbien,

interface of ethernet 1 and 2 are interchanged.

Ethernet 1 is XETH2, Ethernet 2 is XETH1

maurusbien
Established Member

Re: Static IP Address WebPanel WR21

Hello,

plaese find attached some pictures of the configuration. I connect the ctrlX HMI Device to an ctrlX CORE X3 with the networkconfig 192-168.1.1/16 on XF10.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist