Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

parameters and firmware storage

parameters and firmware storage

Sophie
Community Moderator
Community Moderator

Where are the parameters and the firmware stored?

5 REPLIES 5

Mr_SafeMotion
Community Moderator
Community Moderator

=> Parameters and firmware for the ctrlX DRIVE are stored in the device directly.
Not in the display like in IndraDrive.

Parameter and firmware will be "portable" from one drive to the other with the optional ctrlX DRIVE Panel.
There is no additional MMC/SD card in the drive. There is only a SD card in combination with a ctrlX CORE.

aFouraker
Occasional Contributor

@Mr_SafeMotion, I see that you can backup parameters from a drive but does the utility to restore the parameters from the display to a drive exist?

Drives_Uwe
Community Moderator
Community Moderator

Yes, the function to restore the parameters from the panel to the drive exists as a beta or prototype version. Please address to your sales contact in case you need this function.

Hi, may I know if the function of loading parameters from the panel to the drive is still only available in beta?

CodeShepherd
Community Moderator
Community Moderator
Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist