FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
07-07-2020 03:19 PM - edited 07-08-2020 10:56 AM
Where are the parameters and the firmware stored?
Solved! Go to Solution.
07-08-2020 10:55 AM
=> Parameters and firmware for the ctrlX DRIVE are stored in the device directly.
Not in the display like in IndraDrive.
Parameter and firmware will be "portable" from one drive to the other with the optional ctrlX DRIVE Panel.
There is no additional MMC/SD card in the drive. There is only a SD card in combination with a ctrlX CORE.
08-17-2023 05:43 PM
@Mr_SafeMotion, I see that you can backup parameters from a drive but does the utility to restore the parameters from the display to a drive exist?
08-23-2023 06:02 PM
Yes, the function to restore the parameters from the panel to the drive exists as a beta or prototype version. Please address to your sales contact in case you need this function.
4 weeks ago
Hi, may I know if the function of loading parameters from the panel to the drive is still only available in beta?
4 weeks ago
Please have a look to "Parameters settings in display from the drive in case of exchange".