cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

maximal DC Voltage at XCS

maximal DC Voltage at XCS

stefanAT_ctrlX
Long-established Member

Hello,

I have a XCS with an external brake resistor and a MS2N motor. The maximal DC voltage adjustment for the motor is 950V (P-853).

On the DC-Bus we have also an external equipment (load) which works with maximal 800V DC. Therefore I want to limit the DC output of the XCS drive. I can adjust the switch on limit for the resistor (P-834) to e.g. 730V but the P-853 (I adjust to 790V) will be set automatically while switching to OM to 950V  (from the motor /encoder feedback). What can I do.

st_ctrlX_user_0-1677592296967.png

 

Regards, Stefan

1 REPLY 1

Drives_Uwe
Community Moderator
Community Moderator

There is no need to change the parameter P-0-0853 to a lower value than 950V. The bleeder will correctly be switched on at 730V as parameterized.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist