FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
09-09-2024 04:45 PM
Hello,
I'm trying to execute backup and restore in the panel of ctrlX Drive. When I try the backup option (any of the three options), the panel freezes and seconds later resets, without making the backup.
The versions that I have are these:
-ctrlX Drive Version: FWA-XD1-AXS-V-0602N-NN-00
-Panel Version: FWA-XD1-PAN-V-0118.00
-Language Version: FWS-XD1-LIN-ES_____-NN-V-0112
Any ideas?
09-11-2024 12:19 AM
You need another panel firmware if you have a drive with SMO. Address to your application contacts at Bosch Rexroth to get this version.
09-12-2024 07:40 AM
Hello,
The drive doesn't have SMO.
10-07-2024 10:13 AM
3 weeks ago
Hello @Drives_Uwe,
I have used the files you attached but it doesn't work, the panel freezes and seconds later resets when I activate the backup. Exactly the same thing happens with the versions that I posted in the first message (Panel-V0118.00, Axis-V0602 and Language-V0112 ES). I have tried it with two different drives (without SMO) with two different panels and the result is the same, the backup cannot be done.
3 weeks ago - last edited 2 weeks ago
Please send as well the drive parameter file in format "all parameters". Because maybe there is something wrong there.
Strange thing is: in all my tests the backup/restore was functioning with this new panel firmware I sent to you.
Do you know how to correctly install both the panel and the language version files to the panel using a USB connection?
3 weeks ago
2 weeks ago
Is my understanding correct that it was not working as you used Spanish as language for the panel?
2 weeks ago
Yes, this is it!!