cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

ctrlX DRIVE - DoubleAxis - is it possible to have STO Option T0 and SMO Option M5/M8 in one device ?

ctrlX DRIVE - DoubleAxis - is it possible to have STO Option T0 and SMO Option M5/M8 in one device ?

ChrM
Established Member

With IndraDrive both axis in one device coud be either Lx or Sx - only.

In future the granularity of different options - for example SIL3+ are very expensive with M8-HW and SIL3+ SW Option on the SMO - so the second axis in a double axis device should be possible to get as M5 or T0 safety option. 

And how can it be referenced in the type code of the double axis?

1 REPLY 1

Drives_Uwe
Community Moderator
Community Moderator

In the very moment this is not foreseen. In a double axis the safety option is always valid for both axes.

Recommendation: Use single axis drives to differentiate the safety options for the single axis.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist