FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
05-23-2024 04:39 PM
05-24-2024 07:32 AM
Please give us some information what the "ErrorID" and "ErrorIdent" is, to check what is happening.
Which function block is used for writing the parameter/executing command? I guess "IL_ECATSoeCommand".
What is current state of drive when command is executed?
05-24-2024 08:17 AM
Did you checked by Drive Engineering (parameter editor) that the S197 (command C3300) is available in the drive?
05-24-2024 09:12 AM
In Drive Engineering, I am not able to find S197, it looks like it doesn't exist in the Drive.
05-24-2024 09:21 AM
3 weeks ago - last edited 3 weeks ago
I have tested it with 0404 and S197 is available. See attached screenshot