cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

S-0-0197 - Command C3300

S-0-0197 - Command C3300

Quentintin
New Poster

Hello,

I am looking to find this command in a ctrlX Drive with ctrlX Core.

Configuration :
- X3 : 2.04
- ctrlX Drive : 4.02

I try to write this command (C3300) in the Ethercat with my program but an error occurs.
If I try an other command (like C0300), it works.

What can I do ?

5 REPLIES 5

CodeShepherd
Community Moderator
Community Moderator

Please give us some information what the "ErrorID" and "ErrorIdent" is, to check what is happening.

Which function block is used for writing the parameter/executing command? I guess "IL_ECATSoeCommand".

What is current state of drive when command is executed?

Trumpf_Gunnar
Established Member

Did you checked by Drive Engineering (parameter editor) that the S197 (command C3300) is available in the drive?

In Drive Engineering, I am not able to find S197, it looks like it doesn't exist in the Drive.

Yes, I use IL_ECATSoeCommand.

The drive is in standstill during the execution of the command.

I have tested it with 0404 and S197 is available. See attached screenshot

Trumpf_Gunnar_1-1718004098636.png

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist