Reference of paramter P-0-0383

Reference of paramter P-0-0383

alink
New Contributor

Hello,

I'd like to calculate an average energy consumption of drives.

To avoid too much complexity, I'd like to use parameter P-0-0383. With this parameter there is the energy consumption since comissioning. But this is a addition of consumption over the whole lifetime and less useful. To get a more useable value this should be devided with working duration time.

But there are two times:

P-0-0190 for controler - time (power on time +24VDC)

P-0-0191 for time with power on (power on time 3x230VAC)

More interesting is time with power on. But which reference is P-0-0383 using, complete time from P-0-0190 or power on time P-0-0191?

 

But first there is another issue: How to read out P-0-0383 in PLC it seems it is not available.

Thanks in advance

1 REPLY 1

alink
New Contributor

OK, meanwhile I found another parameter which is available in PLC, P-0-0819.

If I'm right, than this is energy consumption just when power on (3x230VAC) and not with controler power (+24VDC).

But I wonder, why is P-0-0383 available in IndraWorks / ctrlXDrive but not in PLC?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist