10-26-2022 03:39 PM - edited 10-26-2022 04:53 PM
Hello,
I'd like to calculate an average energy consumption of drives.
To avoid too much complexity, I'd like to use parameter P-0-0383. With this parameter there is the energy consumption since comissioning. But this is a addition of consumption over the whole lifetime and less useful. To get a more useable value this should be devided with working duration time.
But there are two times:
P-0-0190 for controler - time (power on time +24VDC)
P-0-0191 for time with power on (power on time 3x230VAC)
More interesting is time with power on. But which reference is P-0-0383 using, complete time from P-0-0190 or power on time P-0-0191?
But first there is another issue: How to read out P-0-0383 in PLC it seems it is not available.
Thanks in advance
Solved! Go to Solution.
10-26-2022 05:12 PM
OK, meanwhile I found another parameter which is available in PLC, P-0-0819.
If I'm right, than this is energy consumption just when power on (3x230VAC) and not with controler power (+24VDC).
But I wonder, why is P-0-0383 available in IndraWorks / ctrlXDrive but not in PLC?